Test Parameters
The available parameters vary depending on the selected test.
| AC(V) | Set the AC voltage of the step. Number next to AC represents the phase number. |
| DC(V) | Set the DC voltage of the step. Number next to DC represents the phase number. |
| Duration(s) | Set the step execution time in seconds. This also controls the V Ramp and F Ramp time when those options are selected. |
| AC V Ramp | Enable or disable the AC voltage ramp. When enabled, AC voltage signal change linearly over the specified time instead as a step. |
| DC V Ramp | Enable or disable the DC voltage ramp. When enabled, DC voltage signal change linearly over the specified time instead as a step. |
| Freq (Hz) | Set the step frequency in hertz. |
| F Ramp | Enable or disable the frequency ramp. When enabled, frequency signal change linearly over the specified time instead as a step. |
| Output | Turn the output on or off. |
| Wave | Select the waveform bank number (ID) for the step. To select previously-stored waveform bank, open the waveform bank setting file beforehand. See Open Waveform Bank Setting File. You can also customize and directly select the waveform bank. See Customize Waveform. |
| Jump | Skip steps, enter the destination step number. |
| Loop | Set the number of times to repeat the step continuously. |
| 12 Phase (°) | For 3 phases output, set the phase 1 and phase 2 angle difference. |
| 13 Phase (°) | For 3 phases output, set the phase 1 and phase 3 angle difference. |
| TriggerOut | Turn the trigger out signal on or off. When the trigger signal output is turned on, the signal is output for several tens of microseconds when a step is executed. |
| StatusOut | Turn the status signal output on or off. When the status signal output is turned on, the signal is output only while the step’s waveform is being output. |
| Status | Display results upon completion of the step. |